Installing and maintaining lighting in industrial facilities is often a complex and costly task, as the majority of the fixtures are in dangerous and difficult to reach locations. Elevated mounting heights, obstacles, and other challenges can drive up both the dangers and the costs associated with these tasks.
Be sure to evaluate a luminaire’s mounting and wiring features. A well-designed light can reduce installation effort and significantly lower labor costs. This is especially important with retrofit projects, where labor costs are a key factor.
Mounting styles | Simplified retrofits | Reduce installation effort | Eliminate dangers
Fixture location placement and the proper mounting height are essential to designing a lighting installation that provides uniform illumination with minimal glare and light trespass. The numerous mounting styles available from Eaton’s Crouse-Hinds Division offer unparalleled flexibility, ensuring that the fixtures are installed in the correct location to properly light your application.
Crouse-Hinds series LED luminaires utilize the same mounting modules as our legacy HID, fluorescent and incandescent products, simplifying installation and significantly reducing costs in retrofit projects. We also offer mounting adapters and kits for quick connection to other manufacturers’ modules.
We engineer our LED luminaires to be as installation-friendly as possible. The features below help reduce installer effort, stress, and potential injury.
For lights in elevated locations, OSHA/HSE regulations require fall prevention equipment any time a worker is exposed to a fall of six feet or greater. Since 2000, the #1 most frequently violated OSHA standard each year is General Requirements for Fall Protection. And while personal protection equipment will help protect workers from threat, there is still a risk of injury from a fall. Preventing the worker from being exposed to the threat altogether is the most effective risk-reduction measure.
Safety lowering poles are an effective way to transition from protecting the worker to eliminating the risk. By enabling the luminaire to be lowered, the safely pole allows all installation or maintenance work to safely take place on the platform or walkway. This eliminates the timely and costly need for fall protection equipment and portable ladders or scaffolds.
Safety lowering poles are a good option for industrial lighting applications in hard to reach areas, as well as for any luminaires installed on walkways, platforms, stairways and conveyors where OSHA/HSE regulations require fall prevention equipment.
Our patent-pending V-Spring light poles increase safety and decrease labor costs associated with lighting installation and routine maintenance.
This LED Lighting Design and Specification Guide details key factors to consider when selecting a manufacturer for industrial lighting, and demonstrates how Eaton’s Crouse-Hinds series LED solutions are built to withstand the toughest conditions, deliver maximum lighting performance and safety, and reduce expensive maintenance costs.