The B-Line series slide assemblies are designed to support pipe where horizontal movement from expansion and contraction is present.
The B-Line series pipe alignment guides are used to help direct thermal expansion of insulated or non-insulated pipe in the direction permitted by expansion joints or loops. The use of two or more guides on both sides of an expansion joint or loop is recommended. Pipe lines should be supported with hangers or rollers so that when properly installed, the guides will not be supporting any pipe loads.
Eaton offers a wide variety of pipe slide and guide options in various materials, finishes and sizes.
For a full line of pipe slides and pipe guides, view or download the pipe hanger catalog.