Location: Vestaburg, Michigan
Segment: Potato harvesting
Challenge: Assist in developing an all-hydraulic version of an airhead-type harvester that would deliver improved performance, streamline the manufacturing process and increase productivity.
Solution: Eaton® EFX CAN controllers and tandem Eaton DuraForce® hydrostatic transmissions.
Results: The all-hydraulic design has reduced the number of man-hours required to assemble the airhead, while the electronics have greatly enhanced the machine's capabilities.
Eaton's CANBus system eliminates a lot of wiring, about three or four thousand feet per machine. The plumbing is a lot simpler as well. For example, the electronically controlled pumps only deliver the amount of power that's needed, so they generate a lot less heat. There is no wasted flow, which greatly reduces fuel consumption and reduces operating costs.
Potatoes are harvested by digging them up and separating them from rocks, soil and other field debris. This process makes delivering an un-bruised potato a significant challenge, one that has been met and largely overcome by engineers at Advanced Farm Equipment (AFE) in Vestaburg, Michigan.
AFE developed an airhead-type hydraulic potato harvester, which is a sophisticated, selfpropelled machine designed specifically to harvest potatoes with an absolute minimum of bruising.
An AFE airhead-type machine is a complex, diesel-powered potato harvesting factory on wheels that has revolutionized the way potatoes are harvested. As the machine moves down a row, the potatoes, rocks, earth and other field debris are lifted and placed on a conveyor. Potatoes are separated from rocks and dirt as they pass under a vacuum that “levitates” the potatoes while allowing the rocks (which are heavier than the potatoes) to fall, hence the “airhead”designation.
“This is a very temperamental operation,” said Greg Merrihew, AFE manager, “that requires fine adjustment to compensate for factors including humidity, wind direction, the size and quantity of rocks in the field and many other constantly changing conditions. Our original machines used a lot of belts, pulleys and chains.
“We depended on varying engine speed, or mechanically changing pulleys and sprockets to accommodate changing conditions. They worked very well, and still do, but we are always looking for better ways of doing things.
“We had a lot of experience with hydraulic fan drives and other sub-systems over the years, so when it came time to upgrade the airhead system we began seriously looking at an all-hydraulic machine.”
DTS Fluid Power, an Eaton distributor in Grand Rapids, Michigan, has been supplying hydraulic components to AFE for the airhead machine and other equipment for many years. DTS engineers worked with Merrihew’s design team to develop an all-hydraulic version of the airhead-type machine. The new version utilized the latest technology to deliver improved performance while streamlining the manufacturing process and increasing productivity.
“Eaton is one of the primary proponents of merging hydraulics and sophisticated electronics into integrated electro-hydraulic systems,” explained DTS’ Trent Tegg, vice president of sales and marketing. “Eaton offered a single source for nearly all of the hardware and software AFE needed to produce a really revolutionary product – everything from the programmable touch-screen display in the cab to the high-performance pumps, motors, and valves that make things happen deep in the heart of the beast.
“It’s all tied together with Eaton EFX CAN controllers that communicate with device-mounted electronics via a single CANBus cable. The machine can be pre-programmed to match the user’s exact conditions, and the operator can change functions on the fly as things change.”
Among the advanced hydraulic technologies included in AFE’s upgraded airhead-type machine are a pair of tandem Eaton DuraForce hydrostatic transmissions. A product resulting from an alliance between Eaton and Linde, DuraForce pumps, motors, valves, and transmissions represent the next generation of super-efficient, high-pressure hydraulic technology.
“DuraForce products are a natural choice for this application,” Tegg said. “They are cutting-edge technology based on proven designs that deliver both efficiency and reliability, in a compact package, with great controllability.”
The switch to an all-hydraulic design controlled via CAN and CANBus wiring has reduced the number of man-hours required to assemble the airhead, while the electronics have greatly enhanced the machine’s capabilities.
“Eaton’s CANBus system eliminates a lot of wiring,” Merrihew said, “about three or four thousand feet per machine. The plumbing is a lot simpler as well. For example,the electronically controlled pumps only deliver the amount of power that’s needed, so they generate a lot less heat. There is no wasted flow, which greatly reduces fuel consumption and reduces operating costs.
“The machine is a lot more capable now because the operator can adjust virtually everything from the cab. Of course, that also means it’s easier to get into trouble, so we have programmed a lot of fail-safes into the system and provided pressure reliefs so things aren’t torn up if a stone gets caught or some other mishap occurs. We have developed pop-up troubleshooting screens that pinpoint any potential hydraulic or electrical problems and have incorporated horsepower management controls so nothing is ever put at risk.”
Perhaps the most important advantage of the new technology is the fact that AFE can monitor and troubleshoot the machines in real-time via a cell phone connection or the Internet. In addition, the machines automatically log operating data that is also available for download.