Biesse’s world-leading woodworking machines are
the first to update their pushbuttons by installing
Eaton’s latest Flat Front Design technology.
Location: Pesaro, Italy
Segment: Machine Building
Challenge: The quality and standards of the machine required updates and modernizing
Solution: Install innovative, reliable and aesthetically pleasing pushbuttons
Results: A cost-effective design that vastly improves the user experience and adds value to the entire machine
The quality and user experience provided by Eaton's innovative RMQ Flat Front command devices, and the accessibility that the new Biesse dashboard provides enables the user to really feel the quality of the entire machine.
Challenge
Simplify and improve the user's life, safety and enjoyment of the machine
Biesse initially approached Eaton to discuss the company's need to revise the general aesthetics of its woodworking machinery. In particular, both parties identified that the most important aspect of any redesign would need to focus heavily on the user's experience of the machine. This is because the machine's interface with the operator is what gives the user the most amount of feedback on the quality of the machine in its entirety.
So the overall objective of the project was to find pushbuttons for the operator that had an innovative look and feel. Their fronts needed to be flat and aesthetically pleasing, in line with wider developments and trends in the market, as the most common style of pushbuttons that protrude from the machine's dashboard has become obsolete on their machines.
Biesse pays a great deal of attention to the type of experience the user has when interacting with its machinery. Which is why the user' experience, reliability and aesthetically pleasing design were paramount considerations when looking for the new pushbuttons to integrate on the new machines.
"Biesse needed to rely on a partner who could offer 360- degree assurances: a partner that boasts a whole range of automation products and that could deliver quality products sourced globally," notes Alberto Carrotta, Automations Manager at Biesse. "This is why we chose to work with Eaton, as both our companies share the same goals: we are both geared to innovation and able to offer advanced solutions."
Carrotta also stresses that Biesse's dashboard designs are very similar on all of its machines. "This simplifies the user's life, as they rapidly learn to interact with and safely use the basic functions on machines belonging to different manufacturing processes. So, for example, the start and stop functions on all Biesse machines are performed in the same way."
Finally, the solution had to be competitive in the woodworking segment. At the same time it needed to be easy to install and had to meet the highest IP standard. Which is why, until very recently, it was still uncommon to see pushbuttons that, as well as being appropriate for industrial applications, were as beautifully designed as those that you find on an elevator, or in other areas of life.
Solution
A cost-effective, safe and innovative design that delights the user
The new range of Eaton RMQ Flat Front pushbuttons offered Biesse the ultimate compromise between quality, reliability and enjoyable user experience. Reliability, in particular, is of paramount importance.
In its procurement phase, Biesse required the suppliers for each component that would be installed on its machines to offer a guaranteed number of operations. The technology offered by the new RMQ AFX mounting system adapts automatically to different sheet metal thicknesses, which makes installation faster and more reliable. Additionally, the innovative RMQ Flat Front models can be combined with Eaton's new RMQ-Titan and RMQ compact range providing great flexibility when it comes to designing machines.
"The simplest selector switch must always be able to transmit the desired command to the machine and an emergency stop pushbutton must be available at any time to stop the machine immediately, if necessary," Carrotta explains. "A machine operator's user experience is of vital importance to Biesse and even a simple pushbutton must perform its own work impeccably."
Results
A delightful user experience
Biesse successfully demonstrated Eaton's RMQ Flat Front pushbuttons design at the world's leading woodworking fair, XyleExpo, a vitally important opportunity for the company to stand out from the crowd. Eaton's RMQ pushbuttons on the control panels were a key component in helping Biesse's machines stand head and shoulders above its competition.
"Most importantly, from the point of view of the device's aesthetically pleasing design, the Eaton pushbutton, thanks to the attractive design with a satin metal ring and its compactness, has been considered to be the one that offers the user the best experience in terms of look and feel," says Paolo Valentini, Manager of Industrial Design & Engineering at Biesse.
"Within the woodworking market, Biesse was one of the first companies to pay close attention to the aesthetic pleasure of the machines. And, as you can see from the results of the collaboration with Eaton, Biesse still works in this direction today, offering 'functional design' that is suitable for the industry but is, at the same time, safe and enjoyable for our users."
Background
Biesse Group is a global leader in technologies for processing wood, glass, stone, plastic and metal. It designs, manufactures and distributes machines, integrated systems and software for manufacturers of furniture, door/window frames and components for the construction, ship-building and aerospace industries. Founded in Pesaro in 1969 by Mr. Giancarlo Selci, Biesse has been listed on the STAR segment of Borsa Italiana's equity market since 2001.
Biesse Group has four business areas (Biesse, Intermac, Diamut, Mechatronics) and ten manufacturing facilities in Italy and abroad.. It is one of the global leaders in the woodworking market and the first Eaton customer to install it's latest RMQ Flat Front pushbuttons.
Biesse and Eaton have worked closely together to successfully improve the human-machine interface of its woodworking machines using the very latest Flat Front Design technology.