Combining 100 years of transmission expertise with the latest in IoT technology to help drivers reduce unplanned downtime and stay safe on the road.
Without Eaton’s remote diagnostics system in place, fault codes are collected and sent to a fleet’s existing telematics provider. From there, the codes are distributed directly to fleets without any analysis or immediate, actionable next steps.
IntelliConnect remote diagnostics provide the Intelligent Power advantage. Here's how it works.
All Eaton and Eaton Cummins automated transmissions on a vehicle with supported telematics devices will have fault codes evaluated by IntelliConnect on the fly. The evaluated information from IntelliConnect is sent to fleet managers, supplementing data already received from the telematics service provider. The data is first collected in our knowledge management system. IntelliConnect monitors the fault codes, identifies the critical errors impacting the driveline and then ranks them by severity. After that, a fault code action plan is generated and sent to the appropriate system users in the fleet via email alerts.
You decide what, when and how you receive information.
IntelliConnect is just one example of the impact the Internet of Things (IoT) has on how you can use insights to drive efficiency and productivity. Learn more about our approach to IoT.